Hello,
I am using this module to charge the 3.8V 385mAh battery. I have set the VBATREG at 4.35V. But the charger doesn't reduce the current at 4.35V. It continue charging till 4.5 V.
I have setup the register as below.
VBAT_CTRL = 0x4B ( VBATREG = 4.35V)
ICHG_CTRL = 0x9A (ICHG = 192.5)
TERM_CTRL = 0x2A (21% of ICHG)
All other registers have the default values. After reading in datasheet I found that I have set the PMID voltage to 4.5V. And the recommended value is 200mV higher then the VBATREG. but by I2C I can only set it to 4.4V. Is there any hardware setting I can do to set the PMID to 4.37V.
And Please let me know if is there any other changes require to fulfil the charging condition.
Thank you.