Other Parts Discussed in Thread: BQ7718, BQ2947, BQ2945
Hi Team,
I would like to know if BQ7692003 can support 2 cell LifePO4 battery. The 2 batteries with 3.2V nominal voltage will be mounted in series which will be 6.4V in total. The discharge voltage for each is 2.5V and will be 5V in parallel for both.
Is there a way for BQ7692003PWR to support 2 cells? the datasheet specifies that the minimum is 3 Cells and that the minimum voltage required to make the IC works properly is 6V and the discharge voltage is 5V. or can you recommend a device that can support this?
Thanks in advance.
Regards,
Marvin