Part Number: TPS2419
Hi All,
We've recently integrated a TPS2419D ideal diode controller along with it's N-channel MOSFET into a DC/DC schematic
While it does work a treat at first start (powering the DC/DC via it's 48V HV input), it's the second time I get a weird behaviour (gate = 0V all the time) on some edge cases.
The thing is :
- The DC/DC is being shut-down by opening the negative side (via a photoMOS relay)
- The DC/DC is NOT isolated
- We need to apply 12V first (from an external source) onto the +12V OUT in order to start and then control the SSPC by putting it's pin 2 (Cathode of the emitting LED) to the ground.
- The TPS2419D seems to be working correctly at first but then we apply 12V at the input (or we open the 48V GND) and it's then down
What I suspect : when the +48V GND is left floating, we get some strong common-mode that is enough to fry the chip.
Hereafter is a screenshot of the schematic, please bear in mind the Schottky Diode has been added as a safety measure to be able to get the card working (at the expense of a big thermal constraint).