This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3686: how can I get 2.5V and 1.2V output

Part Number: LM3686
Other Parts Discussed in Thread: LM3687

Hi experts,

about LM3686, does the output voltage adjustable? how I can get stable 2.5V and 1.2V output, when input 3.0V-4.4V.?

how about LM3687, can I get stable 2.5V and 1.2V output?

Thanks.

Anderson

  • Hi Anderson,

    These are legacy devices with limited support available.

    LM3687 is a fixed output device, more information can be found on page 4 of the datasheet.

    LM3686 does not have any information I am able to find about configuring the output voltage options.

    Best regards,

    Layne J