Other Parts Discussed in Thread: BQEVSW, BQ40Z50, GPCRB, BQ20Z45, BQSTUDIO
I have a battery pack that uses a bq20z45-r1 that jumps zero SOC when the temperature drops to 0C or lower.
I did not have anything to do with the design of this battery pack but several years ago I did some work with a BQ 27510 and I have used BQ software (I have bqEVSW 0.9.90) software and the necessary hardware to interface to the bq20z45-r1 gas gauge in the battery pack. All the settings I see in the BQ software seem to only protect the battery against over and under temp when charging but I do not see any register that specifics a low temperature cutoff on discharge.
What we saw was the battery was reporting around 75% SOC at 1C and a couple min later the temp dropped to Zero C and the SOC started reporting zero SOC but the battery was still running in our system as expected based on the battery being around 75% SOC actual.
We would like the battery to operated at -20C so is there a setting or a register I could change to get the gas gauge report the actual SOC down at these lower temps?
Thanks,
Doug