Other Parts Discussed in Thread: TIDA-010247
Hello,
We are using stacked bq76952 configuration as per TIDA-010247 reference design. Up until now we've been balancing alternate cells, recently we decided to use the adjacent cell balancing feature.
When 2-3 adjacent cells are being balanced it works fine, but when the number of balancing cells increases further the AFE starts to overheat and reach around 90-100 degree Celsius (Observed via thermal camera), and the internal temperature cutoff of the AFE turns off the balancing.
We are using Rbal = 22 Ohm, Rn and Rn-1 = 100 Ohms, Rgn = 10 kOhm and Cn as 220 nF
The Gate Threshold voltage of the external NFET is ~0.8V
And the input cell voltage was around ~ 4V
What would be your recommended solution for this
Thank you