Hi All,
I have a question about the output voltage of UCC28911.
I want to input 280V DC and output 54V DC, but according to WEBENCH, the maximum VOUT is 25V.
Is it possible to output 54V with UCC28911?
Best Regards,
Ishiwata
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi All,
I have a question about the output voltage of UCC28911.
I want to input 280V DC and output 54V DC, but according to WEBENCH, the maximum VOUT is 25V.
Is it possible to output 54V with UCC28911?
Best Regards,
Ishiwata
Hi JCHK-san,
I think it depends on the peripheral components, but is it possible to use DC54 output with DC280V input without any problems as a product specification?
Customer plans to use UCC28911 for battery charger.
Best Regards,
Ishiwata
HI Ishiwata-san,
You are correct in that this is a function of the peripheral components. The limitation you will run into is the total amount of power that can be delivered.
I submitted the request to fix Webench yesterday so it will allow this once it gets refreshed.
I hope this answers your question.