This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65217: TPS65217 IC

Part Number: TPS65217

We are using your TPS65217 IC in one of our project .We are getting one issue in field side that boards becomes non-functional .After checking we found that Octavo processor SYS_VOUT pin is unable to produce 5V .

 

As per PMIC datasheet, brownout condition will come when 5 V is dropped below 3.3V under voltage lockout and recovered before reaching 100mV. In this scenario, PMIC is not able to detect power rise and remains in lockout condition.

 

Since Octavo has  TPS65217 IC as PMIC which can enters   into lock up when below condition comes.

 

This condition comes very rare but we want to solve this issue but unable to reproduce this issue at our end ,can you please help us how we can create this issue  in our board.

 

Regards,

Vipin