This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76952: Design Stackable BMS using TWO BQ76952 IC. Need you support to remove LD Pin Circuit.

Part Number: BQ76952
Other Parts Discussed in Thread: TIDA-010247

Dear TI team,

I am designing 24S BMS using your reference design TIDA-010247, I don't want to use the LD pin circuit mentioned in your design ref some requirement issue. 

So can tie the LD pin of both AFE to each ground directly & DNP some components as I attached. 

1) D22 replace with 0ohm resistance.

2) D20 replace with 0ohm resistance.

3) DNP: R148,D21,Q41,R149,Q46,R156,D25,R164,R155,D24,R163,D23

.