This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76940: BQ76940 initilization abnormal in -10 ℃

Part Number: BQ76940

Dear Sir

The recent test found that when BMS is below -10 ℃, (it is no problem for the temperature to recover above 0 degrees) after AFE enters Shutdown Mode and wakes up through TS1 pin, MCU cannot initialize AFE successfully, resulting in failure of reading voltage, current and temperature.
However, the REGOUT voltage of 3.3V has been normal, we have removed C11 and C15, it should be OK, we are still analyzing and solving, and the samples from the customer are still suspended
The question is: When the power supply is normal, why does the initialization fail? Is it risky to get rid of C11 and C15? thank you!

  • Hello,

    Do TS1, TS2 and TS3 have a thermistor or pull down resistor? This is required as per datasheet. 10k is the recommended value.


    Is it risky to get rid of C11 and C15?

    The datasheet does not mention these are a must. You can do some test, but they don't seem to be required.

    This is an useful E2E thread about wake up issue.

    Regards,
    Jose Couso