Part Number: BQ34Z100EVM
Other Parts Discussed in Thread: BQ34Z100
Hello,
I'am using the BQ34Z100 EVM board, when I load the content of the data flash subclass ID 48, its content is not organized as discribed in the datasheet of the bq34z100 and the bq34z100-g
As exemple, the design capacity at offset 11 is stored at offset 21, cell charge voltage T1-T2 and T2-T3 are at offset 28-29 30-31.
All the data of te subclass ID48 are shifted by 10 bytes.

Until now, I didn't see another problem in the other subclasses.
Can you hlep to understand what happen?
if its can help, the control command returned following data :
device type : 0x0100
FW_Version : 0x0006
DF_version : 0x0000