This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS53355: TPS53355DQPR about reel specifications

Part Number: TPS53355

What are the reel specifications when ordering the TPS53355DQPR?
If one reel has 2,500 pieces, is the reel width W1(mm) 15.4[mm] or 12.4[mm]?
The datasheet listed his two specifications for the TPS53355DQPR.