Hello!
I have a question about the PMIC clock.
A crystal was connected to OSC32KIN/OSC32KOUT as with the evaluation board. (same model number)
I measured the waveforms of the clocks and both output waveforms had a maximum of 400mV.
As far as I can see from the data sheet, the OSC32KIN/OUT voltage uses VOUT_LDOVRTC as the power supply, so I think the input will be about 1.8V, but is there no problem with an output of 400mV?
In addition, I recognize that there is no problem because the PMIC sequence switches from OFF to ON in the time as designed.
best regards,