Other Parts Discussed in Thread: TPS54218, TPS54318, TPS54319, TPS54320, TPS54418, TPS54521, TPS54618, TPS54620, TPS54622, TPS548B22, TPS548C26, , TPS548D22, TPS53355, TPS546D24A, TPS548D21
Hi Ti Team,
We are using the part TPS54623RHLR for the below mentioned speciation's :
VOUT = 1.8 V
Rise Time = 10 ms
Monotonicity = 0 mV
Slope = 7120 V/s
Tolerance = +/- 10%
Ripple = 20 mV
Overshoot = 50 mV
Overshoot settling time = 0.05 ms
Iout = 0.56 A
we have tried many ways to optimise the Overshoot Settling time but we could optimise, kindly share your valuable inputs to optimise the Overshoot Settling Time.
for this design the desired Overshoot Settling time 0.05ms we could optimise upto 0.36ms.
Master key : 0F0F4E54B4813362[v1]