Hello,
I am working on a project where i have to perform ring communication between BQ79652 and BQ79612 ICs. I have connected the COMH of upper device to COML of lower device. But i cant wake up the stack device. I am sending a Wake ping by pulling the Receiver pin of BQ79652 low for 3ms and then added a delay of 12ms*total boards. I have used the same code for daisy chain and it was working but for ring communication it's not working.
Is this the correct wake sequence for ring communication? Thanks.