Can more than one TPS7H2221-SEP load switch be placed in parallel to increase max current?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Can more than one TPS7H2221-SEP load switch be placed in parallel to increase max current?
The correct part number i am looking at is the TPS7H2221-SEP.
Hi Craig,
Yes, more than once device can be paralleled in order to increase the total current.
Part-to-part differences in R_ON will mean the current may not be shared equally between devices though, so this should be accounted for when designing so that the max current rating (1.25A) is not exceeded for any individual part.
Thanks,
Sarah