Dear Team,
Problem facing: IC is not generating the switching pulse at SW pin even after providing the CTRL pin PWM signal.
Please provide any solution.
Input conditions:
1) CTRL Pin input frequency 20Khz, 80% duty cycle. with 3.3V level
2) VCC+5V with 2 Amps capability,
Circuit Components:
1) Input capacitor 4.7uF/25V
2) Inductor 10uH / 450mA
3) MBRAF440T3G DIODE SCHOTTKY 40V 4A
Backlight LED of Display:
1) 3 LED's in series and same pair repeated 10 times in parallel.
2) Each LED 3.2V forward drop and total current consumption is 200mA