Hello -
I'm using the LM61495Q3 in a design as implemented in the schematic is attached below. The input voltage range is 24V to 33V and the output voltage is 24V. I have the enable pin (EN, pin 13) connected to a microcontroller to control power on/off. The symptoms I see are:
- Voltage out is the same as voltage in. Tested input range is from 25V to 31. Regardless of Vin, Vout is the same as Vin.
- The voltage at the feedback pin (FB, pin 7) is 1.27V. I thought for adjustable output, the reference voltage is 1.0V.
- The EN pin is controlled by the microcontroller: When Ven = 0V, the output of the converter is 0V as expected. When Ven = 3.3V, the output of the converter is Vin.
- RESET is always low whether EN is high or low. So
I tried increasing the voltage on the EN to 6Vand 9V with the same results. It was not clear to me Ven,min is from the datasheet but I interpreted it as anything above 1.365V should be good. I have not applied a load to the output yet. That's the next step but I thought it would convert the voltage even at no load.
I'm sure I'm missing something but have failed to find it. Any input would be greatly appreciated.
Thanks,
Todd