Other Parts Discussed in Thread: BQ25792,
As stated in the title we are looking to use a BQ25792 or BQ25798 to power a device that will require 3V at around 50 micro amps most of the time with a high current draw around 300-400mA infrequently (less than 1 time a day for a short period) on battery power. These ICs were chosen because the application is outdoor and requires the batteries to be monitored for temperature during a charge to stay within recommended limits.
We need to use a very small PV panel only capable of supplying around 1-1.5w of power due to space constraints. Currently looking at a 9V 100mA to stay above the 3.5 Vmin for a longer period of time during daylight. Could potentially go a little bit larger on the PV panel but it would still be well under 500mA.
So, the first question is, can a Lion or LiPo be "trickle" charged from this small of a solar cell using either of these ICs? Or if not able to charge the battery, at least be able to offset power usage of the board during the day?
The board will also randomly be hooked to a 24VDC source that can be as high as 28-30 volts depending on the alternator/batteries connected.
Should a regulator be installed before the chip to trim that voltage down to the Vmax of 24 or can they use this power supply as is below the absolute Vmax of 30?
Links to a similar reference design would be extremely helpful as well.
Thanks,
Jacob