This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2662: Power Oring application

Part Number: TPS2662

Hello Experts,

We need your assistance to check our customer schematics. I have posted their inquiry here.

In my new design, I am planning to use two TPS26621DRC components for the PowerOring application. There are two inputs rail:7V2_BAT_F - from 5V to 8.4V; 11V_EXT_PS_F - from5 to 16 volt.  VBAT_EXT is combined output. The maximum current did not exceed 700mA. The FLT output is connected to enable other components on other pages; the pull up located there.   Attached electrical schematics. Could you comment on the implementation?

TPS26621_oring (1).pdf

Thank you in advance.

Best regards,

Jonathan