Hi team,
I am working on BMS with 48V, 60A rating. I want to explore this active pre charging circuit for my application
I am not able to understand few things in the schematic.
1. As we have to charge capacitor till rated voltage, Vcap= 400V, but inductor side of R6 is grounded. How current will flow and voltage will build up? Please excuse me but I am not able to get it.
2. This is high side side drive circuit as load is connected to source, but UCC27517AQDBVRQ1 is low side driver.
3. Once the capacitor is charge, we should not turn on the precharge circuit. Do we have to use voltage measurement at capacitor?
It would be really helpful, if you can elaborate.
Thanks and regards,
Monica