This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5012: Vout drop after increasing the load

Part Number: LM5012
Other Parts Discussed in Thread: LM5013

Hi team,

My customer designed a circuit that Vin=48V, Vo=24V, Io=2.5A. And Vo stays normal of 24V when with no load.

But Vo will drop to 18V when increasing the load to 2A. Below is the SW scope in LM5012 @ 2A.

And when they change LM5012 to LM5013, Vo will be a slightly higher than 24V when increasing the load to 2A.

Could u kindly help to explain the possible reason and do u have any advice on the drop of LM5012?