Part Number: BQ76942
Hello,
If none of the BQ7694201's internal LDOs (REG1, REG2) are configured. Does the SPI bus use REG18?
If so, is it push-pull or open drain configuration for the MISO pin.
Alternatively can REG1 be externally powered from an external regulator to force SPI to use REG1.
I am interfacing the BQ7694201 via SPI to an STM32 and am deciding whether I need a level shifter or I can get away with direct connections.
Cheers,
K