Part Number: BQ24192
Hello Team,
We are using a BQ24192 battery charger in our system with the following configurations.
- The Battery is connected to the output of BQ24192 with an additional fuse in the series.
We are facing an issue with the battery charge voltage, battery charging is getting stopped at 3.9V instead of 4.2V.
Do we need to change any register settings due to the addition of the fuse in series with the battery?
For reference, I've also attached the register settings that currently we are using.
| REG00 | 0x2F |
| REG01 | 0x10 |
| REG02 | 0x90 |
| REG03 | 0x11 |
| REG04 | 0xB3 |
| REG05 | 0x86 |
| REG06 | 0x03 |
| REG07 | 0x40 |
| REG08 | Not Using |
| REG09 | Not Using |
| REG0A | Not Using |
Kindly refer and help to debug the issue.
Thanks,
Kaushal