This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27411-G1: BQ27411-G1 Programming OTP using MCU

Part Number: BQ27411-G1
Other Parts Discussed in Thread: BQ27542-G1, , BQSTUDIO

Hello TI Team,

We were using battery fuel gauge part No: BQ27542-G1 and now since TI is not promoting this part, we got suggessition to use part number BQ27411-G1 which is best fit for BQ27542. However, during our analysis it is observed that the new part (BQ27411-G1) has OTP memory and need to write it with .OTFS file.

Will you please suggest can we write .OTFS file into the OTP memory using host controller(MCU) in production without using SmartFlash sotware. If yes, is there any sample code available to write OTP memory using host controller? And can you please provide us code to integrate in our application.

Aslo, the OTP programming document says that this device need to supply with 7.4V during programming. Please confirm if that is mandatory or any other voltage level which can be used to program the device?