Hello,
I am designing a 2.4 kW PSFB DC-DC Converter. I am using UCC28951. I have used the excel tool provided during my power stage design, and I also used the values of the compensation network from there. I have attached the excel file that contains all my specs.
I am having a difficulty making the converter stable. I see a lot of noise on my current sense signal even though I have a low-pass filter in there. I am unable to exceed 10 A on the output without having stability issues. Also the same at no load. The problem becomes more pronounced, the more the input voltage is increased.
These are my measurements.
Yellow : Output voltage
Light blue : Voltage on the primary side of the transformer
Red : Drain-Source voltage of one of the switches
Green : Gate-source voltage
Yellow : Current sense pin
Dark blue: Current in the primary side of the transformer.