Other Parts Discussed in Thread: CSD19534KCS
5241.TL494 BOOST CONVERTER.pdf
The above is a circuit diagram of the BOOST CONVERTER using the designed TL494.
1. Operational problems
1.1 When power is applied, MOSFET is damaged, S and D are shorted, and power supply CC operation
1.2 Same phenomenon with SMD type NVMFS5H663NL MOSFET
2. It is judged that the specifications of the elements are not lacking, is there any problem with the circuit problem with the circuit?
3. Also, Inductor L1 is built with IDC 30A at 68uH, R6,R18 uses current sensing resistance from GMR320HJAAFD5L00, F1 to F5 used NFM41PC155B1H3 EMI filter.
4. Designing a High Power, High Efficiency Boost Converter using TL494 (circuitdigest.com) I referred to the link.