Part Number: TPSF12C3QEVM
Please advise how you derived the inductance value for the filter’s LCM1 and LCM2 of AEF. Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPSF12C3QEVM
Please advise how you derived the inductance value for the filter’s LCM1 and LCM2 of AEF. Thanks.
Hi Lucas,
The values for Lcm1 and Lcm2 depend on the EMI noise source amplitude and the allowable Y-caps. If you have an existing passive filter design that passes, then the chokes are typically be 4-5 times lower in inductance (based on the amplification of the Y-rated inject cap by AEF).
Regards,
Tim
Is there a possibility to get the relation between the EMI noise source amplitude and the allowable Y caps in an excel file or formulae?
Do we have an orderable reference design part number for this board?
Thanks.
Project information (3):
Project 3ph 460Vac input, 4.5kW, Iline = 7.7Arms max
Project 3ph 230Vax input, 4.5kW,Iline = 15Arms max
Project 1ph 230Vac input, 4.5kW,Iline = 25Arms max
Hello Lucas,
The value of the Y caps is normally set by touch current limitation. The formula is approximately Maximum Y capacitance = 10 nF * touch current spec. 60 Hz, 240 V input assumed. Once you have a value for Y capacitance, this capacitance can be distributed between sense and injection capacitors. With typical gain, about 30, 150 mV should be assumed for maximum allowed center node ripple with AEF on. This sets the minimum Lcm2 value. Use 30 x inject capacitance as the Y capacitance for this calculation.
The board shown is not yet orderable so we will have to send one to you manually. Please email Sharadh Navale, and my self to request a board.
Regards, Robert