Other Parts Discussed in Thread: BQ24172, BQ77915
Hi Ti team,
Hopefully a simple one, regarding the BQ24170 battery Charger IC.
We have designed the BQ24170 set for a 3-Cell (Series) Charger at 12.6V using 18650 3000mAh Cells.
We also have a tap off of the lowest cell in the string to create an Auxiliary 3.3V supply (powering a signal relay), which has a current draw of 65mA.
The lowest cell will continue to discharge, powering the signal relay after a full charge cycle.
Theoretically, we expect the charger to restart once the voltage dips below a threshold.
What we are experiencing is the charger does not re-attempt a Recharge cycle and goes into a FAULT state anywhere between 1-2 days after power up.
The new good cells all sit at ~ 3.7V/cell before power up. After the FAULT state occurs, the cells out of the circuit measure anywhere from 0V (open-circuit), <1V, or as high as 4.6V/cell.
Additional note we are also using the BQ24170 on multiple products with no issues, no FAULTS, and all Recharging cycles are okay, only difference on this product is the 3.3V AUX tap from the lowest cell in the string.
In theory, we expect a recharge cycle to attempt periodically, if we could have some clarification around the fault/issue that would be great.
Look forward to hearing back.
Kind regards,
Daniel