Other Parts Discussed in Thread: BQ79600-Q1
HI,
I AM Sudhir and my question is if i'm using three stack devices ,and using daisy chain ,may i use TX RX pin of the base device to the microcontroller directly for CAN communication.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI,
I AM Sudhir and my question is if i'm using three stack devices ,and using daisy chain ,may i use TX RX pin of the base device to the microcontroller directly for CAN communication.
Hi Sudhir,
Yes, you are able to use the TX RX pin of the base device to the MCU for CAN communication.
Best Regards,
Julia Louis
IF I USE BQ79654-Q1 as a stack device (three stack 14 cell each) then which should be as a base device .
any other ic like bq79600 is called base device here or botom stack device is base device?
Hi Sudhir,
If the BQ79654-Q1 device is utilized as a stack device, you have a couple of options for your base (bridge) device.
Best Regards,
Julia Louis