Hi Guys,
I trust you are well.
I'm using the TPS61235 as part of an IOT board.I'm powering the converter from a 3.7v 21700 5Ah LiPo battery. The schematic is attached below:

I have done the following checks so far:
(1) Confirmed that the enable pin is high
(2) Vin applied is greater than the minimum Vin specified in the datasheet.
(3) Isolated the output of the regulator from the rest of the circuit to eliminate the possibility of any loading related issues preventing startup.
Do you guys have any suggestions regarding the potential causes of the output voltage being 0.3V.
Kind Regards,