Part Number: TPS2062C-2
Hi Team,
Why TPS2062C-2 need to add 150uF at the output? Seem the output power is not very bigger.

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS2062C-2
Hi Team,
Why TPS2062C-2 need to add 150uF at the output? Seem the output power is not very bigger.

Hi Kevin,
Greeting!
You can refer to the below description in our datasheet, the root cause is the requirement in HUB application, if you are not the HUB application, just need one 10uF and one 0.1uF are ok, thank you.

Best Regards,
Kuno
Hi Kuno,
Could I know that why need to add an 120uF at HUB application? Thanks.
Hi Kevin,
It seems for the Inrush Current limit, you can refer to the below USB2.0 spec. Thank you.


Best Regards,
Kuno