Other Parts Discussed in Thread: CSD18514Q5A, CSD17579Q5A
- This is a sinusoidal inverter.
- Supply: 12V to 24V DC RMS, 100W
- Input: I'll drive the PWM generator with a 100 kHz sinewave.
- If the sine is 100 kHz, the PWM needs to be high enough to give a clean, low-EMF sine on the output. I don't know if Nyquist is sufficient, or higher. Affects output filter. 1 Mhz is a guess.
- I'll drive the Mosfets with the PWM generator.
- Load: Hungry inductive power load that wants up to 20A, 5V AC power, continuous.
- Actually, four parallel inductive loads at up to 5A ea. They are coupled inductors.