Hi Expert team,
I want to use a coupled inductor in SEPIC configuration of LP8866-Q1 backlight driver. In datasheet or on e2e I did not find any related topic to understand the requirement for this. is there anything I need to take care in schematic as well as in layout while using coupled inductor? Please help.
The basic requirements are
Vout= 35.2V
Vin(min)= 9V
Iout = 780mA
Fsw = 1818KHz