Other Parts Discussed in Thread: , LM5143, TINA-TI
When I use LM25149EVM board,I change output voltage to 25.2V(by change R20 and R21).
EVM board works good,but L3 is hot when loading 6A(temperature of L3 >100℃,ambient temperature is 25℃).
Then I chang switching Frequency to 500kHz(by changing R13 to 42K),when power up,it looks good,but there is a noise sound.
After 3 seconds,board shutdown,Q1 and Q2 burned.
Two Questions:
Why Q1 and Q2 burned?
And I want to simulate LM25149 Loop stability(gain margin and phase margin),how to simulate?