This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP87642Q1EVM: Default JSON file for this EVM

Part Number: LP87642Q1EVM

I have one of this EVM. But I do not have a default JSON file for default program that is executing this EVM.

Please share theJSON file for this EVM. Thanks

This is a 4 phase single output design. When I try to create such a design with Scalable PMIC GUI software, I am not sure why Buck3 and Buck4 monitor options show up under the "BUCK" tab.

Bala

  • Hello Bala,

    You can see options for BUCK3 and BUCK4 monitors because when the regulators are configured in 3-phase or 4-phase configurations, the UV/OV voltage monitors of BUCK3 and BUCK4 regulators can be used to monitor external supply rails. Please have a look at section 7.3.2.1.4 in datasheet for more information.

    We will get back to you within 24 hours about the configuration file for the EVM.

    Thank you for your patience,

    Florian

  • Bala,

    Please find attached the file you requested.

    https://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/196/LP876411E2RQKRQ1_5F00_rev0_5F00_2022Feb8.json

    Best regards,

    Florian