Other Parts Discussed in Thread: LM74502-Q1
Hi,
Regarding the LM74502H-Q1 device and this schematic;
1) Is this device suitable for automative oil/water pump application?
150W motor, 12V Battery, 13A rated with 40-50A peaks.
Must be protected against to the typical surges on automotive power rail (in picture).
2) Is there available Grade0 alternative of this IC or will it be available in future?
3) Without the TVS diode, like in the schematic,
What could be the expected behaviour with ISO7637 pulse 1 transient?
Is it possible to simulate this device with that ISO pulse and see the voltage stresses at each node?
4) If the TVS is mandatory for -150V pulse (expected the positive pulse protected up to 100V),
is it possible to use only a unidirectional TVS to protect negative only?
5) In the overvoltage clamp mode, switching of the mosfet should require any EMC concerns?
If yes is there any recommendation for suppression of the switching noise?
6) Is there any issue with the 40V Q2 FET usage when the overvoltage limited at 28V like in the schematic?
What could be the formula between the min Q2 FET voltage and Overvoltage limitation?
7) For the FETs, RDSon must be selected as low as possible but is there any limit or consideration for the gate charge?
8) Is there any comment on the 50V capacitor usage?
Regards