Hello,
We want to discharge the battery as it is plugged into the charging board, but I am concerned the BQ chip could sink current and become damaged since the BATFET body diode would allow current to flow to SYS. Our discharge current is not high, maxing out at 160mA. Do we need to modify the design to use the OTG function and have the second input source be the discharge circuitry, or is there a way to put the BAT pin of the BQ25792 into a high impedance state and prevent current flowing through the IC? I do not see way to set the charger to output 0mA in the data sheet ( the lowest output current seems to be 40mA). I believe setting the BQ chip to the lowest current setting would work but am not sure if that is advisable for the health of the IC.
Thanks,
Peyton