Hi,
I would like to confirm which silk screen printing in the following pictures is commercial grade? Which screen is industrial grade?
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Rhea,
Both devices are commercial grade. In general, we do not classify devices as industrial grade. Our commercial devices typically meet the required temperature range of industrial grade devices.
While both devices you've shared are technically commercial grade, N05B is rated to a operate over a wider temperature range, -40°C to 125°C. N05A is rated to operate from 0°C to 125°C.
I hope this is helpful. Please let me know if I can clarify anything.
Erin
Hi Erin,
I believe you said 06A and 06B. Thanks for your answer, I know that the temperature range of B is larger.
Mainly depends on whether the temperature meets the requirements of the working environment.
Thanks again!