This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5143-Q1: When EN enable, MOS will damage

Part Number: LM5143-Q1

hi team,

now customer use LM5143-Q1,meet a problem, this case is very urgent.

device work condition: VIN =24V, Vout=14.4v, the typ Iout=6A.

when customer enable the EN, the mos of Vout2 will breakdown.

of course customer test when remove MOS of Vout1 or Vout2, this circuit can work normal.

the attached file is schematic, could you help support this problem.G3_SCH_0305(3).pdf