Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92560: Boost Constant Current getting fried directly after powering up

Part Number: TPS92560

Hello!

I am trying to design a LED replacement board for 12V GY6,35 Halogen lamps. My design uses a Osram Duris S10 LED, which is supposed to be driven with 38 V and a constant current of 100 mA.

This is the schematic of the board:

I've taken the design and component values of the TPS92560 Component Calculator.

Sadly, the TPS92560 gets extremely hot as soon as the 12 V AC are connected.

After assembling a completely new test pcb and double-checking all connections and parts, I do not have any clue what could be the issue.

Any help or suggestions are appreciated!

Best regards,

Jelko