Other Parts Discussed in Thread: BQ25570, BQ25504,
Hello.
The BQ25570 circuit I asked you about earlier works well because the problem has been solved.
When applying mass production products, the circuit is changed, so the output of BQ25570 is not required, so we would like to change it to BQ25505 or BQ25504 to reduce the cost of parts.
I can't decide which one suits my purpose, BQ25505 or BQ25504, so please advise which one would suit me better.
1. Li-po 130mAh Li-Po
2. 3.3V OUTPUT PMIC
3. 2.4V Indoor Small Solar Cell
In addition, I would like to ask if it is correct to attach a diode to the battery input and output as shown in the picture.
Regards,
JP