This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25896: Does BQ25896 support to hot plugin of battery pack?

Part Number: BQ25896

Dear Ti support team.

I made a battery charger system by BQ25896. Does BQ25896 support to hot plugin of battery pack when dc power is suppleid ?

The battery pack is having +,TH,-.And single cell.

Battery connector doesn't have sequence pin. So, 3 Pins is same length.

  • Hello, 

    Thank you for reaching out via E2E. Unfortunately, there is not a straightforward answer on this. The BAT pin is rated for 6V. Care must be taken to ensure good transient characteristics (< 6V) during the hot plugin event. If hot plugin with your specific battery pack does not result in transient spikes of 6V then it should be no problem for BQ25896.

    Best Regards,

    Garrett