Other Parts Discussed in Thread: TPS61021A, PSPICE-FOR-TI
Hello Texas Instruments Community,
good day,
I want to design two groups of LED drivers with reference to PMP15037, but TPS61021A can only provide 1A driving current, and the driving current I need is 1.5A and 2A, so can I directly use TPS61023 instead of direct design?
Input power supply: 3V;3.7V
Output power: 3.5V@2A;4V@1.5A
In addition, can I simulate this design method on PSPICE-FOR-TI, because now I also encounter problems like "PSpice model ERROR(ORPSIM-16592)"