I have a custom designed PD using TPS2376-H. I implemented only Mode B PoE whereby power can only be delivered over spare pins since this part will only go into my own system. I have a switch that can operate in Mode B. (Ultimately I am going to redesign PD to be fully compliant, but wanted to at least make sure my handshake worked on this rev). However, when I plug ethernet in and scope the PoE output, I seem to be getting stuck in detect stage and never leave. My detect resistor combined with UVLO resistors give 24.9k and I verified with meter. Attached is my schematic for the PoE portion of the circuit. I have auxiliary power diode-or'd in and have verified that the rest of my board works fine. Have also used a PoE injector to just put power through my diode bridge and board works fine there as well. PGOOD signal goes to DCDC enable. A bit stuck on what to try next. Also attached my scope screenshot of PoE signal. It ramps up to 5V, then ramps again to 10V and repeats forever. Switch I am using is GSD-504UP from Planet Tech. Any help greatly appreciated.