Hello, thanks in advance for your help with the TPS7H5001. I have a few questions on the error amplifier and the CS_ILIM.
1. What is the input voltage common mode range where the parameters of the error amplifier are guaranteed?
2. What is the range of the error amplifier?
3. The CS_ILIM has a top limit of 1.05V for protection. What is the hysteresis margin?
4. Is this device set or reset dominant? The block diagram does not show the set-reset latch.
Thanks for your help,
Jorge Vega