Other Parts Discussed in Thread: TPS6594EVM
Hi Team.
I am designing a circuit using the TPS6594****.
And I think that the TPS65941319/TPS6594133A is suitable because the BUCK configuration in NVM is 2+1+1.
So here's the question.
Q1) NVM is only for initial settings, and I think that the settings can be changed arbitrarily via I2C after the TPS6594 starts up. Is this correct?
(For example, voltage value, slew rate, GPIO settings, etc.)
In other words, regardless of NVM-ID (TPS6594****), can it be used in the same way by register settings?
Q2) Where are the primary and secondary settings?
Thank you.