Hello,
I have to design a 50/100 A current source, from a power sypply of 14/18 V.
The load is resistive and with that current should not be more than 10/12 V.
I'm searching for a controller when I can set the desidered current with an MCU.
The LM5170 has all the specifications I need for my project, but It works between two voltage port HV and LV (2 batteries tipically).
I don't understand if it can works between a power supply on the HV port and only a resistive load in the LV port.
Please, can you give me some informations about?
Thanks in advance