This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2521: About clamping the output

Part Number: TPS2521

Hello,

I would like to ask you about the TPS2521.
(Question 1)
My specs expect a maximum of 5.4V on the IN pin.
The load current at that time is 15mA.
Since VCLAMP=5.0V(min), I think that (5.4V-5.0V)×15mA=6mW loss always occurs.Is this idea correct?
(Question 2)
In Figure 7-22 on page 13 of the data sheet, up to a load current of 1000mA, how much will the clamp voltage drop at 1.5A, 2A, and 2.5A?

Best regards,