Other Parts Discussed in Thread: TPS2660, SN74LVC1G14
Hi Team,
Can you suggest most simple power mux with TPS2640 ( there is no need for fast switchover time). ( eg FLT and SHDN pin)
Input 1 ( Always has priority)
Vin1 from 12V to 24V
Input 2
Vin2 from 5V to 25V - but it should only work from 12V to 24V ( when 5V then it is UV lockout activated)
-> when only input1 connected it powers output from 12V to 24V
-> when only input2 connected it powers output from 12V to 24V ( 5V to 12V is in UVLO)
-> when input1 and input2 connected, if input1 (from 12V to 24V) then input1 powers output regardless of input2 voltage
-> when input1 and input2 connected, if input1 (in UVLO or OVP state) then input2 powers output .
In this case when input 2 powers output and input1 in UVLO, will the current flow from input2 to input1 through reverse current blocking mosfet of the efuse1 ?
Best Regards,
d.